DINT to String (DTOS)

This information applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers.
The DTOS instruction produces the ASCII representation of a value.
Available Languages
Ladder Diagram
DTOS_LD_avail lang_v31
Function Block
This instruction is not available in function block.
Structured Text
DTOS(Source,Dest);
Operands
Ladder Diagram and Structured Text
Operand
Type
Format
Description
Notes
Source
SINT
INT
DINT
REAL
Tag
The tag that contains the value
If the Source is a REAL, the instruction converts it to a DINT value.
Destination
String type
Tag
The tag to store the integer value
String types are:
  • default STRING data type
  • any new string type you create
Description
The DTOS instruction converts the Source to a string of ASCII characters and places the result in the Destination.
Affects Math Status Flags
No
Major/Minor Faults
Type
Code
Cause
Recovery Method
4
51
The LEN value of the string tag is greater than the DATA size of the string tag.
Check that no instruction is writing to the LEN member of the string type tag.
In the LEN value, enter the number of characters that the string contains.
4
52
The output string is larger than the destination.
Create a new string type that is large enough for the output string. Use the new string type as the data type for the destination.
See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
N/A
Rung-condition-in is true
The instruction executes.
Postscan
N/A
Structured Text
Condition
Action
Prescan
See Prescan in the preceding Ladder Diagram table
Normal execution
See rung-condition-in is true in the preceding Ladder Diagram table.
Postscan
See Postscan in the preceding Ladder Diagram table
Example
When temp_high is set, the DTOS instruction converts the value in msg_num to a string of ASCII characters and places the result in msg_num_ascii. Subsequent rungs insert or concatenate msg_num_ascii with other strings to produce a complete message for a display terminal.
Ladder Diagram
DTOS_LD_ex_v31.png
Structured Text
IF temp_high THEN
DTOS(msg_num,msg_num_ascii);
temp_high := 0;
END_IF;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal