Bit Shift Left (BSL)

This table lists the controllers and applications that support this instruction.
Architecture
Standard applications
Safety applications
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes
No
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Yes
Yes
The BSL instruction shifts the specified bits within the Array one position left.
When enabled, the instruction unloads the uppermost bit of the specified bits to the .UL bit, shifts the remaining bits one position left, and loads Bit address into bit 0 of Array.
IMPORTANT: You must test and confirm that the instruction does not change data that you do not want it to change.
The BSL instruction operates on contiguous data memory. The data is constrained by the specified member.
In this transitional instruction, the relay ladder toggles the rung-condition-in from false to true for the instruction to execute.
Available Languages
Ladder Diagram
Operands
Ladder Diagram
Operand
Type
Format
Description
Array
DINT ARRAY
tag
Array to modify
specify the first element where to begin the shift
Control
CONTROL
tag
Control structure for the operation
Source Bit
BOOL
tag
Bit to shift into the vacated position.
Length
DINT
immediate
Number of bits in the array to shift
CONTROL Structure
Mnemonic
Data Type
Description
.EN
BOOL
The enable bit indicates the BSL instruction is enabled.
.DN
BOOL
The done bit is set to indicate that bits shifted one position to the left.
.UL
BOOL
The unload bit is the instruction’s output. The .UL bit stores the status of the bit that was shifted out of the range of bits.
.ER
BOOL
The error bit is set when .LEN < 0.
.LEN
DINT
The length specifies the number of array bits to shift.
Affects Math Status Flags
No
Major/Minor Faults
A Major Fault Occurs If
Fault Type
Fault Code
The LEN exceeds the size of the array
4
20
See Common Attributes for operand related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The .EN bit is cleared to false.
The .DN bit is cleared to false.
The .ER bit is cleared to false.
The .POS value is cleared
Rung-condition-in is false
The .EN bit is cleared to false.
The .DN bit is cleared to false.
The .ER bit is cleared to false.
The .POS value is cleared.
Rung-condition-in is true
See BSL Flow Chart (True).
Postscan
N/A
BSL Flow Chart (True)
Examples
Example 1
When enabled, the BSL instruction starts at bit 0 in array_dint[0]. The instruction unloads array_dint[0].9 into the .UL bit, shifts the remaining bits, and loads input_1 into array_dint[0].0. The remaining bits (10-31) are invalid.
Ladder Diagram
Example 2:
When enabled, the BSL instruction starts at bit 0 in array_dint[0]. The instruction unloads array_dint[1].25 into the .UL bit, shifts the remaining bits, and loads input_1 into array_dint[0].0. The remaining bits (31-26 in array_dint[1]) are invalid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal