Corrected anomalies in this release
This list identifies the anomalies that are corrected in the Logix Designer application version 37.00. Use the identification information provided in parentheses to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
General
Uploading a project from the controller sometimes fails (3314529)
When you attempt to upload a project from a controller running Logix Designer versions 34, 35, or 36, the upload sometimes fails.
This anomaly corrected in version 37.00.
This anomaly first identified in version 34.00.
Toggle Inline Value Display feature can cause Logix Designer to shut down (3818739)
The Logix Designer application can become unresponsive or shut down when you use the
Toggle Inline Value Display
setting while these conditions are true:
- You are viewing the logic of an AOI that references at least one Logix tag-based alarm.
- The AOI logic is in a structured text routine.
The error can occur when you are either offline or online with the controller.
This anomaly corrected in version 37.00.
This anomaly first identified in version 31.00.
HMIBC tags permitted in 5580 Redundant applications (3396611)
Logix Designer does not prevent you from including HMIBC type tags in Redundant applications, which can lead to controller Primary, Secondary or simultaneous Primary and Secondary assert and errors when you attempt to upload from the controller into an existing or new application when no assert has occurred.
This anomaly corrected in version 37.00.
This anomaly first identified in Logix Designer version 33.00.
Compiler Error When Locking a License-based Source Protected Routine or AOI (3358813)
A compiler error,
Complier Error(0x0A), Call technical support
, appears when trying to lock a license-based source protected routine, where at least one InOut parameter is missing a required connection and that InOut parameter is used in the routine that is being source protected and locked.To work around this anomaly, perform a
Controller Verify
or Build
of the project to determine if any InOut Parameter are missing required connections.This anomaly corrected in version 37.00.
This anomaly first identified in Logix Designer version 32.00.
Fatal Error 0xc0000005 on Import from L5X (3161896)
If an application was generated in an XML editor and a move instruction (MOV/MOVE) was created with an empty/missing operand, a Fatal Error occurs on import of the L5X file.Example of text that would cause the Fatal Error on import:
- <![CDATA[MOV(TagA);]]>
- <![CDATA[MOV(TagA,TagB);]]>
- <![CDATA[MOV(TagA,?);]]>
This anomaly corrected in version 37.00.
This anomaly first identified in version 34.00.
Selecting Go to Cross Ref prompts Save All (3064189)
When you open a project in the Logix Designer application, select
Go to Cross Reference
for a tag, and then close the project, the Logix Designer application asks you to save changes even though the project has not changed.There is no workaround for this issue.
This anomaly corrected in version 37.00.
This anomaly first identified in version 34.00.
"Not enough graphic resources" error when performing a search and replace on a tag (3209190)
When you attempt to search and replace a tag name used in multiple programs, the Logix Designer application sometimes displays an error that states "Not enough graphic resources" and sometimes becomes unresponsive.
To work around this anomaly, intermittently close out tag editor windows during the Search and Replace action to free graphic resources.
This anomaly corrected in version 37.00.
This anomaly first identified in version 31.00.
Opening Extended Properties for new UDT can freeze Logix Designer (3121716)
The Logix Designer application sometimes locks up when you create a new data type and select
for one of the properties.
To work around this issue, hover your cursor over the application icon in the taskbar and close the empty dialog.
This anomaly corrected in version 37.00.
This anomaly first identified in version 36.00.
Partial AOI import sometimes fails to create Alarm (3115573, 2223611)
The Logix Designer application sometimes fails to create an alarm when you do a partial import for an Add-On Instruction (AOI) that contains the alarm.
To work around this issue, export and then import the affected project.
This anomaly corrected in version 37.00.
This anomaly first identified in version 33.00.
Cannot update value for tag member in DT and LDT data types (2363908)
You can expand and display the bit members for tags using the DT and LDT data types, but you cannot change the values for the bit members. This is expected behavior.
This anomaly corrected in version 37.00.
This anomaly first identified in version 36.00.
Unexpected Verification Error on a Signed Structured Text Add-on Instruction (3332140)
The verification error, “Invalid signature ID. Reseal instruction to resolve.” is reported for a Structured Text Add-on Instruction (AOI) that contains a signature and a nested, unsigned AOI. The error appears after edits are made to the unsigned, nested AOI.
To get past the verification error, the signature must be removed and re-added to the AOI with the reported error.
This anomaly corrected in version 37.00.
This anomaly first identified in version 28.00.
Radix Change on Project Upload for Hidden Members of UDT (3084749)
By default, hidden members within a User-defined Data Type (UDT) are defined with a decimal radix. This can be changed in the L5X export of a UDT to another supported radix type.
On project upload, the hidden member tag’s radix would change back to the default decimal style format. This does not affect UDT tag data but could be flagged as a difference when comparing copies of the project file using text comparison tools.
NOTE:
If the UDT is edited within the Logix Designer application, this will also cause the tag’s radix to change back to a decimal style format. Avoid editing the UDT within the Logix Designer application if you prefer an alternative radix for the hidden members.
This anomaly corrected in version 37.00.
This anomaly first identified in version 20.00.
Fatal Error 0xc000005 EXCEPTION_ACCESS_VIOLATION on Upload (3314529)
The Fatal Error occurs on upload if there previously was an Add-on Instruction (AOI) that matched the naming convention from the IEC 61131-3 standard, and that AOI was removed from the project prior to downloading.
To prevent the anomaly, avoid creating AOI mnemonics matching the naming convention from the IEC 61131-3 standard.
This anomaly corrected in version 37.00.
This anomaly first identified in version 34.00.
Devices
Data type fails to change when using certain EDS AOPs (3690460, 3613600)
The following could occur for EDS AOP devices that use a one-dimensional array, with only one element for the input or output tag in their configuration:
- When updating an EDS AOP module’s configuration, it appears that the data type has changed on the module properties, but the update is not present in the tag browser.
- When creating, copying/pasting, or importing/exporting the device, the module-defined timestamps increment for each device created.
This anomaly has been corrected in the Add-on profile Core released with Logix Designer version 37.00.
This anomaly first identified in version 31.00.
Fatal Error When Updating EDS AOP Datatypes (3748086)
A Fatal Error could occur when you select the
Upgrade Data Types…
button for certain EDS AOP device configurations. The Upgrade Data Types…
button is present on the device’s profile if the project environment has been upgraded to support unsigned datatypes. This support was added with the release of Studio 5000 Logix Designer version 36.00.To work around this anomaly, remove and re-add the EDS AOP device to the I/O configuration, which will upgrade the datatype.
This anomaly corrected in version 37.00.
This anomaly first identified in version 34.00.
EDS AOP Module Tags Do Not Reflect Module Definition (3228412)
When you create a new device in the I/O configuration, the module tags in the Controller Tag browser do not reflect the defined module definition.
This can also affect Logix Designer applications with EDS AOP devices that are upgraded to Logix Designer versions 34.00 and later, if Logix Designer version 36.00 or later is installed.
This anomaly is related to the EDS Subsystem installed with Logix Designer version 36.00.
This issue only affects EDS AOP devices in 5380/5480/5580 controller applications.
This anomaly corrected in version 37.00.
See technote
BF30248
for additional information.Adding third-party devices to an I-O Link application sometimes causes Logix Designer to error (3598596)
When you add certain third-party devices to a 5032 I-O Link Master application, Logix Designer could display a Fatal Error or an Invalid Name error, preventing the device from being added to the configuration.
This anomaly corrected in version 37.00.
This anomaly first identified in version 35.00.
Logix Designer version 36.00 installer fails to install AOP Core when GuardLink EIP Scanner AOP is already installed (3193234, 3185534)
When a Guardlink EIP Scanner 432ES AOP version 1.00.34 is already installed on your Logix Designer workstation and you attempt to install version 36, installation errors occur and the installer fails to install AOP core files.
To work around this issue, uninstall the GuardLink EIP Scanner AOP from your Logix Designer application before installing version 36.00. For more information, see
this Knowledgebase article
.This anomaly corrected in version 37.00.
This anomaly first identified in version 36.00.
Event Clear Log button and Display Timestamps are disabled for 5032 IO-Link master and 42AF devices (3127835)
When you open the device configuration page with a 5032 IO-Link Master running with a 42AF IO-Link device at default settings, the
Clear Log
button on the Event Log page is sometimes grayed out. This anomaly corrected in version 37.00.
This anomaly first identified in version 36.00.
Host Words Missing from EDS AOP Module Tags (3597705)
In 5380, 5480, and 5580 controller applications, the Host Words in a tag configuration could be excluded from an EDS AOP device’s Input, Output, and/or Configuration tags. The individual programming bits are still visible.
This anomaly has been corrected in the Add-on profile Core released with Logix Designer version 37.00.
This anomaly first identified in version 34.00.
Provide Feedback