Create a list of options
How do I open the List Editor?
- ClickSETTINGS > Library Attributes.
- Click the ellipsis (...) button next to a setting.
The
List Editor
dialog box is used to create a list of options.To create the list
- Click in the blank space underEnter the strings in the list (one per line). The cursor appears in the box.
- Type the item to include in the list. PressEnterafter each item so that each item is on a different line.
- After all of the items for the list have been entered, clickOK.TheList Editordialog box closes.
Provide Feedback