Update library description

Library Object Manager
supports the library description update of published libraries without creating a library version.
To update library description
  1. In the
    Library Repositories
    column, expand a library repository >
    Libraries
    > library folders.
  2. Right-click the
    Libraries
    node, a library folder, or a library object and select
    Update Description
    .
  3. In the
    Update Library Description
    dialog box, edit the library description.
    TIP:
    Select the
    Libraries
    node or a library folder will update all child library objects' descriptions at the same time.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal