New library settings
The
New Library
dialog box has these settings.Name | Type | Description |
|---|---|---|
01 Library Status | ||
Status | Dropdown menu | If the library is saved as Pending, this revision will be replaced next time changes are saved. If the library is saved as Published, a new revision will be created next time changes are saved. |
02 Revision History | ||
Revision Description | Text entry | A description of the updates made to the current library object, compared to previous versions of the library object. Appears in the Revision History screen when the Object is registered in the Application Code Manager (ACM) application. This is entered manually. This is a required setting. |
03 Library Details | ||
CatalogNumber | Text entry | The library object name, which appears together with the revision number in the library object listing when the library object is registered in ACM. This is entered manually. This is a required setting. |
Description | Text entry | The description of the library object. This is a required setting. |
Family | Dropdown menu or text entry | The family for the library object. This is a required setting. |
Solution | Dropdown menu or text entry | The solution for the library object. This is a required setting. |
Library Type | Dropdown menu or text entry | The library type for the library object. This is a required setting. |
Category | Dropdown menu or text entry | The category for the library object. This is a required setting. |
Content Type | Text | Displays the type of the object. For example, task, program, or routine. |
Owner | Text entry | The user or entity that originally published the library object. This is a required setting. |
Major Revision | Text entry (integer) | The major revision number for the library object. For a new library object, this defaults to 1. |
Minor Revision | Text entry (integer) | The minor revision number for the library object. For a new library object, this defaults to 0. |
04 Library Usage Rules | ||
Upstream Keys | Text entry | For module library objects: a rule that limits the upstream hardware components
that will be made accessible to the library object when it is added to an ACM
Project. The rule is entered manually as a logical expression. |
Downstream Keys | Text entry | For module library objects: a rule that limits the downstream hardware components
that will be made accessible to the library object when it is added to an ACM
Project. The rule is entered manually as a logical expression. |
Provide Feedback