Edit library properties

Use the Edit Library Properties dialog box to edit the properties of the selected library objects. Both pending and published library objects' properties can be edited.
To edit library properties
  1. Select one or multiple library objects.
  2. Right-click one of the selected items and select
    Edit Library Properties
    .
  3. In the
    Edit Library Properties
    dialog box, edit the properties as needed.
    TIP:
    If a parent library object node is selected, select
    Show all Library versions
    .
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal