Copy multiple library objects
Multiple library objects can be imported at one time. Library objects copied from a repository are copied intact. They cannot be edited during the import process.
To copy multiple library objects between folder repositories and the
Application Code Manager
database- Select multiple library objects.
- Hold down theShiftkey to select a contiguous block of library objects.
- Hold down theCtrlkey to select individual library objects that are not contiguous.
- Select a Solution, Library Type, or Category listing to select all of the contained library objects, or select theLibrarieslisting to select all of the library objects in the repository.
- Place the mouse within one of the selected items and drag all of the library objects on top of the folder repository or the ACM database. TheLibrary Import Configurationdialog box opens.
- ClickOKto complete the copy process and publish the library.IMPORTANT:If publishing the library results in duplicated task names, a warning message is displayed. ClickOKto proceed with publishing and accept the duplicate names.
Provide Feedback