Remove the ACM database
Remove an ACM database repository if the database is no longer needed.
To remove the ACM database from the
Library Object Manager
application- In the Library Repositories column, expandRepositories.
- Right-click the ACM database and selectRemove. The ACM database is removed from theLibrary Repositoriescolumn.
Provide Feedback