Connection Properties dialog

The
Connection Properties
dialog box defines the settings for how
Library Object Manager
connects with the ACM database. Use this dialog box to set the data source, the type of user authentication, to specify a different database file, or to modify advanced security settings.
This table describes the settings in the
Connection Properties
dialog box.
Setting
Description
Data source
Database type.
Always select Microsoft
SQL Server
(SqlClient).
Server name
Selects a computer name and
SQL Server
instance from the list or type a computer name and
SQL Server
instance in this format: <Computer Name>\<
SQL Server
Instance>.
Log on to the server
Use Windows Authentication
Allows
SQL Server
sign in using Windows authentication. When selected, the logged on Windows user account credential will be sent to
SQL Server
to authenticate the session.
Use
SQL Server
Authentication
Allows
SQL Server
log on using
SQL Server
authentication. When selected, provide the username and password for the
SQL Server
authentication.
  • User name
    . The
    SQL Server
    username, "sa" by default.
  • Password
    . The
    SQL Server
    password associated with the username specified.
    Starting with Application Code Manager version 5.01.00, the database password is enhanced for security. For more information, see Enhanced SQL Server password management.
  • Save my password
    . When selected, saves the
    SQL Server
    password specified so that it can be used in the next session.
Connect to a database
Select or enter a database name
Select a database name from the list or enter a database name.
Attach a database file
When selected, specify the identifiers for the database file.
SQL Server
database files have two names, the operating system file name used to locate the database in the file system and the logical file name used to identify the database within
SQL Server
transactions.
  • Type a database file name or use the
    Browse
    button to use the
    Select SQL Server Database File
    dialog to locate the database file by clicking through the file system.
  • In
    Logical name
    , type the logical name of the database.
Advanced
Select to configure advanced database properties.
Test Connection
Tests the connection to the database.
If a "Test connection succeeded." message is not returned, check that the following settings are correct:
  • Computer name
  • SQL Server
    authentication
  • Network access (remote
    SQL Server
    )
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal