Advanced Properties dialog

The
Advanced Properties
dialog box provides a means of changing how the connection between
Library Object Manager
and the ACM database passes information.
This table describes the settings in the
Advanced Properties
dialog box. The dialog box is divided into functional areas.
TIP:
Applying the recommended settings will improve ACM performance especially for network connections.
Area
Setting
Possible Values
Description
Advanced
MultipleActiveResultSets
True
False (default)
When True, multiple result sets can be returned and read from one connection.
Network Library
blank (required if local)
Named Pipes (DBNMPNTW)
Shared Memory (DBMSLPCN)
TCP/IP (DBMSSOCN) (recommended if networked)
VIA (DBMSGNET)
The network library used to establish a connection to an instance of
SQL Server
.
Do not use when the
SQL Server
is resident on the local host computer, value should be blank.
Packet Size
8000 (recommended)
Size in bytes of the network packets used to communicate with an instance of
SQL Server
. PacketSize may be a value in the range of 512 bytes and 32,767 bytes.
Transaction Binding
Implicit Unbind (default)
Explicit Unbind
Indicates the binding behavior of connection to the
System.Transactions
namespace.
When set to
Implicit Unbind
, the connection detaches from the transaction when it ends, switching back to autocommit mode.
When set to
Explicit Unbind
the connection remains attached to the transaction until the transaction is closed. The connection will fail if the associated transaction is not active or does not match the current transaction.
Type System Version
Latest (default)
SQL Server
2012
SQL Server
2008
SQL Server
2005
Indicates which server type system the provider will expose through the DataReader.
Connection Resiliency
ConnectRetryCount
2 (recommended)
Number of attempts to restore a connection. The number of reconnections attempted after identifying that there was a connection failure. This must be an integer between 0 and 255. Set to 0 to disable reconnecting on idle connection failures.
ConnectRetryInterval
5 (recommended)
Delay between attempts to restore connection. The amount of time (in seconds) between each reconnection attempt after identifying that there was a connection failure. This must be an integer between 1 and 60.
Context
Application Name
.Net SqlClient Data Provider
The name of the application.
Workstation ID
The name of the workstation connecting to
SQL Server
.
Initialization
ApplicationIntent
ReadWrite (default)
ReadOnly
Declares the application workload type when connecting to a server.
Asynchronous Processing
True
False (default)
When true, enables usage of the Asynchronous functionality in the .NET Framework Data Provider.
Connect Timeout
30 (recommended)
The length of time in seconds to wait for a connection to the server before ending the attempt and generating an error.
A value of 0 indicates no limit, and should be avoided in a ConnectionString because an attempt to connect waits indefinitely.
Current Language
The
SQL Server
Language record name.
Pooling
Enlist
True (default)
False
When
True
, sessions in a Component Services environment should automatically be enlisted in a global transaction where required.
Load Balance Timeout
30 (default)
The minimum amount of time (in seconds) for this connection to live in the pool before being destroyed.
When a connection is returned to the pool, its creation time is compared with the current time, and the connection is destroyed if that time span (in seconds) exceeds the value specified by
Load Balance Timeout
.
A value of zero (0) causes pooled connections to have the maximum connection timeout.
Max Pool Size
1000 (recommended)
The maximum number of connections allowed in the pool.
Valid values are greater than or equal to 1. Values that are less than
Min Pool Size
generate an error.
Min Pool Size
1 (default)
The minimum number of connections allowed in the pool.
Valid values are greater than or equal to 0. Zero (0) in this field means that no minimum connections are initially opened.
Values that are greater than
Max Pool Size
generate an error.
PoolBlockingPeriod
Auto
AlwaysBlock
NeverBlock (recommended)
Defines the blocking period behavior for a connection pool.
When connection pooling is enabled and a timeout error or other sign-in error occurs, an exception will be thrown and subsequent connection attempts will fail for the next five seconds, the "blocking period". If the application attempts to connect within the blocking period, the first exception will be thrown again. Subsequent failures after a blocking period ends will result in a new blocking period that is twice as long as the previous blocking period, up to a maximum of one minute.
Pooling
True (recommended)
False
When
True
, the connection object is drawn from the appropriate pool, or if necessary, is created and added to the appropriate pool.
Any newly created connection is added to the pool when closed by the application. In the next attempt to open the same connection, that connection will be drawn from the pool.
Connections are considered the same if they have the same connection string. Different connections have different connection strings.
Replication
Replication
False (default)
True
Used by
SQL Server
in replication.
Set to
True
if replication is supported using the connection.
Security
Authentication
NotSpecified (default)
SqlPassword
ActiveDirectoryPassword
ActiveDirectoryIntegrated
Specifies the method of authenticating with
SQL Server
.
Column Encryption Setting
Enabled
Disabled (default)
Default column encryption setting for all the commands on the connection.
Encrypt
True
False (default)
When True,
SQL Server
uses SSL encryption for all data sent between the client and server if the server has a certificate installed.
Integrated Security
True
False (default)
Whether the connection is to be a secure connection or not.
When
False
, User ID and Password are specified in the connection. When
True
, the current Windows account credentials are used for authentication.
Password
*******
Indicates the password to be used when connecting to the data source.
Persist Security Info
True
False (default)
When
False
, security-sensitive information, such as the password, is not returned as part of the connection if the connection is open or has ever been in an open state.
TrustServerCertificate
True (recommended)
False
When
True
(and
Encrypt
is set to
True
),
SQL Server
uses SSL encryption for all data sent between the client and server without validating the server certificate.
If
TrustServerCertificate
is set to
True
and
Encrypt
is set to
False
, the channel is not encrypted.
User ID
sa
Indicates the user ID to be used when connecting to the data source.
Source
AttachDbFilename
The name of the primary file, including the full path name, of an attachable database.
Context Connection
True
False (default)
When
True
, indicates that the connection should be from the
SQL Server
context. Available only when running in the
SQL Server
process.
Data Source
localhost\SQLACM (default)
Indicates the name of the data source to connect to.
Failover Partner
The name or network address of the instance of
SQL Server
that acts as a failover partner.
Initial Catalog
Initial Database Name
The name of the initial catalog or database in the data source.
MultiSubnetFailover
True
False (default)
If your application is connecting to a high availability, disaster recovery (AlwaysOn) availability group (AG) on different subnets, setting this value to
True
configures SqlConnection to provide faster detection of and connection to the (currently) active server.
TransparentNetworkIPResolution
True (default)
False
If your application connects to different networks, setting this value to
True
configures SqlConnection to provide transparent connection resolution to the currently active server, independently of the network IP topology.
When set to
True
, the application is required to retrieve all IP addresses for a particular DNS entry and attempt to connect with the first one in the list. If the connection is not established within 0.5 seconds, the application will try to connect to all other IP addresses in parallel. When the first IP address answers, the application will establish the connection with the respondent IP address.
If
MultiSubnetFailover
is set to
True
, this setting is ignored.
If
Failover Partner
is specified, this setting is ignored.
The default setting is
False
if
Authentication
is set to either
Active Directory Password
or
Active Directory Integrated
, otherwise the default setting is
True
.
User Instance
True
False (default)
Indicates whether the connection will be redirected to connect to an instance of
SQL Server
running under the user's account.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal