Add and mount an ACD repository

Create library repositories using an ACD file. ACD files contain controller code for
Rockwell Automation®
Logix platforms, including
ControlLogix®
,
CompactLogix®
, and
FlexLogix
. When basing a library repository off an ACD file, the ACD file must also be mounted in
Library Object Manager
before use.
IMPORTANT:
An ACD file must not be in use when it is mounted in
Library Object Manager
. Before mounting the ACD file, make sure that the ACD file is not open in another application.
To add and mount an ACD repository
  1. In the
    Library Repositories
    column, right-click
    Repositories
    then select
    Add Repository > ACD
    . The
    Select an ACD File
    dialog box opens.
  2. Navigate to the ACD file to add and double-click the listing or click
    Open
    .
  3. The ACD file opens. The file displays with a red "X" next to the name, and that the library objects are not accessible. To make the library objects accessible, the ACD file must be mounted.
  4. In the
    Library Repositories
    column, right-click the ACD file and select
    Mount
    .
  5. The Red "X" no longer displays and the library objects are added to the repository.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal