Remove a folder repository
Remove a folder repository if the folder is no longer needed.
To remove a folder repository from the
Library Object Manager
application- In theLibrary Repositoriescolumn, expandRepositories.
- Right-click the folder and selectRemove.The folder is closed in theLibrary Object Managerapplication and its listing is removed from theLibrary Repositoriescolumn. All library objects that were added to the folder are still present in the folder location and can be registered inApplication Code Manager.
Provide Feedback