View the Logix code

View the Logix code of a library object to review programs, tasks, routines, and linked libraries associated with the object.
To view the Logix code for a library object.
  1. Select a library object in a folder or database depository. The Library Content column and
    Properties
    panel activate.
  2. Click the
    Logix
    item in the
    Library Content
    column. The complete, line-by-line code for the library object displays in the
    Properties
    panel.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal