Update a VBA code item

Add code, delete code or modify the code to upgrade the code item.
To update a VBA code item
  1. Right-click the VBA code item and select
    Update
    . The
    VBA Code Builder
    dialog box opens.
  2. In the
    Select Subroutine/s to Include
    box, select the code item.
  3. In the
    Select Substitutions to Apply
    box, check one or multiple substitutions and click
    OK
    .
  4. Configure the properties as needed.
  5. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal