Delete a message content

Delete one or more messages when they are no longer needed.
To delete a message content from a library object
  1. In
    Library Repositories
    , select the library object that includes the message content to delete.
  2. In
    Library Content
    , expand the
    ME Alarms
    folder and click the
    Messages
    subfolder.
  3. In the
    Properties
    panel, select one message item or select
    Ctrl
    to select multiple items.
  4. Delete items with one of the following methods:
    • Right-click the selected items and select
      Delete
      .
    • Click Delete icon.
  5. In the
    Delete Message
    dialog box, click
    Yes
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal