Extract an attachment
Extract an attachment to copy its original file from an
Application Code Manager
database to a folder on the computer. Extracted files are saved with file names matching their File Name
property.To extract an attachment
- In, selectLibrary Object ManagerAttachments.
- Select an attachment from the list.
- ClickExtract Files.
- InBrowse For Folder, select a folder where the file should be extracted, then clickOK.
Provide Feedback