Delete an attachment reference
Delete an attachment reference from a library in order to stop
Library Object Manager
from exporting and publishing the attachment along with the library.To delete an attachment reference from a library
- In, fromLibrary Object ManagerLibrary Repositories, select a library.
- InLibrary Content, expandAttachments, then select an attachment reference from the list.
- Right-click the attachment reference, then selectDelete.
- When prompted, selectYes.
Provide Feedback