Assign an attachment reference
Assign an attachment reference to a library so that
Library Object Manager
exports and publishes the attachment along with the library.To assign an attachment reference to a library
- In, fromLibrary Object ManagerLibrary Repositories, select a library.
- InLibrary Content, right-clickAttachments, then selectAdd.
- InAdd Attachments, select one or more attachments to reference in the library.
- (optional) Click the ellipsis button(...)next toInclude Conditionto change whenLibrary Object Managershould include the attachment in the library.
- ClickOK.
Provide Feedback