Settings and status in the Control footer
The footer section on the Sequence Control contains the following settings and status indicators.
The communication, failure, and unscheduled/inhibited icons are also displayed in the upper left corner of the diagram window, in the status bar, and on any step or tag the status is detected.
Setting or status | Description |
Zoom control | Adjusts the zoom on the control window. |
Auto-Scroll | Turn Auto-Scroll on or off. |
Sequence name | The name of the Equipment Sequence . |
Status bar | Displays the following status icons: – There is a communication problem with the controller, the SequenceManager server, the live data server, or the tags. – No known communication problem. – There is a failure in the Equipment Sequence . – No known failure in the Equipment Sequence . – The controller is in Program, Remote Program, or an unknown mode. – The controller is in Run, Remote Run, or an unknown mode. – The Equipment Sequence or task is inhibited, or the Equipment Sequence is unscheduled. – The Equipment Sequence is scanning, or the status is unknown. |
Provide Feedback
– There is a communication problem with the controller, the SequenceManager server, the live data server, or the tags.
– No known communication problem.
– There is a failure in the
– No known failure in the
– The controller is in Program, Remote Program, or an unknown mode.
– The controller is in Run, Remote Run, or an unknown mode.
– The
– The