Monitor a step in the Sequence Detail Control
A monitored equipment sequence step shows several functions:
- The user-configured step name and theEquipment Phasename.
- The step execution state.
- If the step is a source or target for a transfer of control.
- If the step has a failure.
- The step is executing.
- If the step or associated phase is paused.

Item | Description | |||
![]() | Failure | Phase failure - generated by the Equipment Phase Failure (PFL) instruction in the Equipment Phase logic.Internal failure - the sequencing engine has encountered a problem with the Equipment Sequence . | ||
![]() | Step Name | The name of the step as configured during creation of the Equipment Sequence . | ||
![]() | Pause status | The symbol shows that:
| ||
![]() | Equipment Phase Name | Each step is configured to reference one phase. The name of the phase is displayed so you know which equipment phase is executing. | ||
![]() | Transfer of Control (TOC) | A step that has been configured as the source to transfer ownership to a following target step, without stopping the execution of the phase. The symbol shows:
When transfer of control is not configured, the symbols are not drawn. | ||
![]() | Step State | When a step is active, and attached to its phase, the step state mirrors the state of the phase. The set of displayed states are: INACTIVE, NOT CONNECTED (active but not attached), IDLE, RESTARTING, RUNNING, RESETTING, HOLDING, STOPPING, ABORTING, HELD, STOPPED, ABORTED, and COMPLETE.
The step state is also represented by the color of the step. |
Provide Feedback



A pause of the phase logic is pending.
An auto-pause of the phase logic is pending.
The associated
The associated