Command a step or Equipment Phase using the Sequence Detail Control
Equipment Phase
using the Sequence Detail ControlCommand an
Equipment Phase
through a step using the Sequence Detail Control.
TIP:
Select
to make a step active.
Active Step Change
Before you begin
- Open a display that contains the Sequence Detail Control.
- TheEquipment Sequencemust be inManualmode.
- The step to be commanded must be active. This implies the step is attached to theEquipment Phaseto be commanded.
To command a step using the
Equipment Sequence
Monitor- SelectTake Ownership
to take ownership of the Equipment Sequence. - Select the active step to see theEquipment Sequencestep command toolbar.
- Select a command to command the equipment phase associated with the step.
- (optional) Once you have completed commanding phases, selectExit Manual
to go back to Automaticmode. - When finished, selectRelease Ownership
.
Provide Feedback