System features
FactoryTalk Design Studio® version 1.03 has these new or enhanced features.
- Restore.Use theRestoreoption to return a project to a committed or saved state to, for example, apply system changes to the committed project.
- Add a project to the FactoryTalk Vault solutionAdd a shared project to the FactoryTalk Vault solution to keep you and your team synchronized by providing a centralized Solution to securely store documents, manage data access, and collaborate on projects.
- Save asUse theSave asdialog box to duplicate a private or shared project.
- DevicesManage devices by:
- Adding and deleting controllers.
- Adding and deleting devices.
- Changing controller and device properties.
- Viewing a device profile.
- Use theDevicesexplorer to view and manage the hardware used in the project.
- UseDevice listto view, edit, and delete devices and to view tags for the devices in the project.
- DSL Reference ManualUse the FactoryTalk Design Studio code editor to view and edit code for FactoryTalk Design Studio elements, including routines, tasks, Add-On Instructions, and FactoryTalk Smart Objects.
Provide Feedback