Known anomalies
Unknown error when creating new project (1991683)
When selecting to create a new project, <FTDS> sometimes shows the error message
Unable to create project
because of an unknown error.To work around this issue, try creating the project again.
This anomaly first identified in version 1.03.
Rejecting new controller in multi-user environment results in orphaned file (2080177)
When working with a shared project, if two users add controllers at the same time, it results in a merge conflict. If the users chooses to accept only one set of changes, they orphan a controller file. The orphaned controller displays as an unassigned device instead of kept as expected. The user must edit the orphaned device in the topology file to assign it.
This anomaly first identified in version 1.03.
Incomplete Devices displayed in Studio 5000 after import the L5X file with duplicated IP (2155910)
After an import of an L5X file with a duplicate IP, the
Devices
list is incomplete.This anomaly first identified in version 1.03.
Provide Feedback