Corrected anomalies
Incorrect error message when creating device with duplicate name (2117249)
In some cases, when trying to create a device with a duplicate name, the incorrect error message
Failed to create new module, Unexpected error writing device
displayed.This anomaly first identified in version 1.03.
Unable to create UDT tag name defined as reserved (1794181)
When creating UDT definitions using a reserved name, such as tag or InOut parameter, you receive a syntax error and the UDT is not created.
This anomaly first identified in version 1.00.
Provide Feedback