XYTraceType constant
Use the constant to specify the trace type.
XYTraceTypeEmpty
(0): Uses the default trace type, Live Data.XYTraceTypeLiveData
(1): FactoryTalk Live Data tags.XYTraceTypeDataLog
(2): FactoryTalk View SE data log model tags.XYTraceTypeHistorian
(3): FactoryTalk Historian tags (or points).XYTraceTypePIServer
(6): PI Server tags (or points).XYTraceTypeDataLogProPlus
(7): FactoryTalk View SE DataLogPro tags.XYTraceTypeAF
(8): FactoryTalk Historian Asset Framework tags (or attributes).Provide Feedback