SetMinMaxUseTag method (XY Plot object)

Uses tags to set the minimum and maximum values of a trace.
Syntax
XYPlot1
.
SetMinMaxUseTag
(
xTagName
,
yTagName
, [
xMinTagName
], [
xMaxTagName
], [
yMinTagName
], [
yMaxTagName
], [
xModelName
], [
yModelName
], [
xTraceType
], [
yTraceType
])
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
xTagName
- is a parameter of String that specifies the x tag of the trace.
yTagName
- is a parameter of String that specifies the y tag of the trace.
xMinTagName
- is a parameter of String that specifies the tag name for the minimum value of the x-axis.
xMaxTagName
- is a parameter of String that specifies the tag name for the maximum value of the x-axis.
yMinTagName
- is a parameter of String that specifies the tag name for the minimum value of the y-axis.
yMaxTagName
- is a parameter of String that specifies the tag name for the maximum value of the y-axis.
xModelName
- is an optional parameter of String that specifies the historical model name. The parameter is required if the
xTraceType
is
TraceTypeAF
,
TraceTypeDataLog
,
TraceTypeHistorian
, or
TraceTypePIServer
.
yModelName
- is an optional parameter of String that specifies the historical model name. The parameter is required if the
yTraceType
is
TraceTypeAF
,
TraceTypeDataLog
,
TraceTypeHistorian
, or
TraceTypePIServer
.
xTraceType
- is an optional parameter of the
XYTraceType
constant. The parameter can be omitted if the trace type is live data or data log.
yTraceType
- is an optional parameter of the
XYTraceType
constant. The parameter can be omitted if the trace type is live data or data log.
Example
Private Sub SetXYPlotMinMaxUseTag() 'Sets the values with tags TagX_Min and TagX_Max for the trace TagX and tags TagY_Min and TagY_Max for the trace TagY of live data. XYPlot1.SetMinMaxUseTag "TagX", "TagY", "{TagX_Min}", "{TagX_Max}", "{TagY_Min}", "{TagY_Max}" 'Sets the values with tags TagX_Min and TagX_Max for the trace Tag1X of PIserver1 and tags TagY_Min and TagY_Max for the trace Tag1Y of PIserver2. XYPlot1.SetMinMaxUseTag "Tag1X", "Tag1Y", "{TagX_Min}", "{TagX_Max}", "{TagY_Min}", "{TagY_Max}", "PIServer1", "PIServer2", TraceTypePIServer, TraceTypePIServer End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal