ResetTagAxes method (XY Plot object)

Resets tag axes in the chart.
Syntax
XYPlot1
.
ResetTagAxes
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
Example
Private Sub btnResetTagAxes() XYPlot1.ResetTagAxes End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal