CurrentYTagName property

Returns the name of the selected y tag. Read-only. String.
Syntax
XYPlot1
.
CurrentYTagName
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
Example
Private Sub GetTagName() Dim str As String str = XYPlot1.CurrentYTagName End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal