CurrentXTagName property
Returns the name of the selected x tag. Read-only. String.
Syntax
XYPlot1
.CurrentXTagName
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.Example
Private Sub GetTagName() Dim str As String str = XYPlot1.CurrentXTagName End Sub
Provide Feedback