CollapseTagList property (XY Plot object)
Returns or sets whether the tag list below the chart will be displayed. Read/write. Boolean.
Syntax
XYPlot1
.CollapseTagList
[= state
]where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.state
- is a parameter of the type Boolean that can be set to one of the following:- True: Collapses and does not show the tag list.
- False: Shows the tag list.
Example
Private Sub CollapseTagList() XYPlot1.CollapseTagList = False End Sub
Provide Feedback