ActiveMarkerColor property (XY Plot object)

Returns or sets the color of the point markers for the selected trace. Read/write. OLE_COLOR.
OLE_COLOR is a type definition that resolves to a Long.
Syntax
XYPlot1
.
ActiveMarkerColor
[ =
value
]
where
XYPlot1
- is the name of an XY Plot object or an expression that evaluates to an XY Plot object.
value -
is an RGB color value that specifies the color of the point marker.
Example
Private Sub SetActiveMarkerColor() XYPlot1.ActiveMarkerColor = RGB(0,0,0) End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal