TrendTraceType constant
Use the constant to specify the trace type.
TraceTypeEmpty
(0): Uses the default trace type, Live Data.TraceTypeLiveData
(1): FactoryTalk Live Data tags.TraceTypeDataLog
(2): FactoryTalk View SE data log model tags.TraceTypeHistorian
(3): FactoryTalk Historian tags (or points).TraceTypeAlarm
(4): FactoryTalk Alarms and Events history.TraceTypeDiagnostic
(5): FactoryTalk AssetCentre diagnostic logs.TraceTypePIServer
(6): PI Server tags (or points).TraceTypeDataLogProPlus
(7): FactoryTalk View SE DataLogPro tags.TraceTypeAF
(8): FactoryTalk Historian Asset Framework tags (or attributes).Provide Feedback