ShowTagList property (TrendPro object)
Returns or sets whether the tag list is displayed. Read/write. Boolean.
Syntax
TrendPro1
.ShowTagList
[= state
]where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.state
- is a parameter of the type Boolean that can be set to one of the following:- True: The tag list will be visible during runtime.
- False: The tag list will not be visible during runtime.
Example
Private Sub ShowTagList() TrendPro1.ShowTagList = True End Sub
Provide Feedback