ControlType property (TrendPro object)
Returns the type of the runtime chart. Currently the only type supported is "
Trend
". Read only. String.Syntax
TrendPro1
.ControlType
where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.Example
Private Sub GetControlType() Dim str As String str = TrendPro1.ControlType End Sub
Provide Feedback