ActiveMarkerColor property (TrendPro object)
Returns or sets the color of the point markers for the selected trace. Read/write. OLE_COLOR.
OLE_COLOR is a type definition that resolves to a Long.
Syntax
TrendPro1
.ActiveMarkerColor
[ = value
]where
TrendPro1
- is the name of a TrendPro object or an expression that evaluates to a TrendPro object.value -
is an RGB color value that specifies the color of the point marker. Example
Private Sub SetActiveMarkerColor() TrendPro1.ActiveMarkerColor = RGB(0,0,0) End Sub
Provide Feedback