TagGroup object

TagGroup object contains a collection of tag objects and provides properties, methods and events that relate to the tag objects. The TagGroup object is used to access tags which you want to read from or write to.
The TagGroup object is not a creatable object. A TagGroup object is accessible through the CreateTagGroup method of the Application object.
Properties
Methods
Events
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal