Tag object

Represents a tag. A Tag object provides runtime information for a tag and allows the value to be set.
It is not a creatable object.
Use the TagGroup object or the
GetTag
and
CreateTag
methods of the TagDB object to obtain a reference to a Tag object.
A Tag object is returned by the TagGroup object's
Add
and
Item
methods. The Tag object does not allow configuration information for a tag to be set.
Properties
Methods
Events
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal