ForeColor property (SignatureButton object)
Returns or sets the foreground color for a SignatureButton object. Read/write. OLE_COLOR.
OLE_COLOR is a type definition that resolves to a Long.
Syntax
object
.ForeColor
[ = value]where
object
– is the name of a SignatureButton object or an expression that evaluates to a SignatureButton object.value
– is an RGB color value that specifies the foreground color for the object.Remarks
For a SignatureButton object, ForeColor returns or sets the color of the text.
Provide Feedback