NumberOfTags property

Returns the number of tags in the HMI tag database. Read-only. Long.
Syntax
TagDB
.
NumberOfTags
where
TagDB
is the global variable
TagDB
. You can also use a variable you have defined as a TagDB object or an expression that evaluates to a TagDB object.
TIP:
If you are not using
FactoryTalk View SE
's VBA, the global variables will not be automatically created and you will have to define your own object variables.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal