DeleteTag method
Deletes a tag from the HMI tag database.
Syntax
TagDB
.DeleteTag
(TagName
)where
TagDB
is the global variable TagDB
. You can also use a variable you have defined as a TagDB object or an expression that evaluates to a TagDB object.
TIP:
If you are not using
FactoryTalk View SE
's VBA, the global variables will not be automatically created and you will have to define your own object variables.TagName
is the fully qualified name of the tag, that is, the path and tag name such as folder1\tag1
.Remarks
- When operating a large amount of data, we recommend that you use the block mode to improve the performance.
- Avoid opening the Tags editor before the operation finishes. Otherwise, errors may occur.
Provide Feedback