TagLabel object
The TagLabel object represents the intrinsic label object. It is not a creatable object. TagLabel objects are accessible through an Elements collection.
The object-specific properties for the TagLabel object are merged with the Element object's properties. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Properties
Methods
Events
Constants
Provide Feedback