Rename tags
Use the
Rename Tag
dialog box to rename tags so that you can import multiple copies of a tag from a network device or another database.The dialog box opens when you confirm to import a tag that is already imported into an HMI project. Because you cannot have two tags with the same name, you must rename subsequent copies of a previously imported tag.
Provide Feedback