Eg: tag placeholders in commands
For the following examples assume that the HMI project contains the following tag references with the following values:
Tag1 = 1 Tag4="Screen2"
Tag2 = 2 Tag5="Display"
Tag3 = 3
The following commands are run from a command line.
Example 1
Display Screen$Tag1$
Result: Replaces $Tag1$ with the tag's value "1", then runs the command,
Display Screen1
Example 2
Display $Tag4$
Result: Replaces $Tag4$ with the tag's value "Screen2", then runs the command,
Display Screen2
Example 3
Set Machine$Tag1$.Motor$Tag2$ $Tag3$
Result: Replaces $Tag1$ with the tag's value "1", replaces $Tag2$ with the tag's value "2", and replaces $Tag3$ with the tag's value "3", and then runs the command,
Set Machine1.Motor2 3
Example 4
Display "Screen$Tag1$"
Result: Command subsystem runs following command (because the quotes indicate a component whose name contains dollar signs),
Display Screen$Tag1$
Example 5
$Tag5$ $Tag4$
Result: Replaces $Tag5$ with "Display" and $Tag4$ with "Screen2" and then runs the command,
Display Screen2
Provide Feedback