Example: HMI tags as an OPC client with an RSLinx OPC server

This is an example to help you set up
FactoryTalk View
as an OPC client with RSLinx Classic acting as an OPC server.
To set up the example:
  1. In the
    Tags
    editor, create an HMI tag with
    Device
    as its data source.
  2. In the tag's
    Address
    field, type
    [Bottling]N7:12
    where
    Bottling
    is the RSLinx OPC/DDE topic and
    N7:12
    - is the OPC item.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal