Symbol Indicator Properties - States tab

The following table shows the options under
Select state
.
Options
Description
Select state
Click the state for which to set up properties. There is also an error state, which is labeled Error.
The following table shows the options under
General
.
Options
Description
Value
Type the integer value to use for each state. You cannot assign a value to the error state (if the object has an error state).
Back color
This field displays the current background color for the state. Click it to select another color.
The following table shows the options under
Image
.
Options
Description
Image color
For monochrome images, this field displays the current image foreground color. Click it to select another color.
Image back color
For monochrome images, this field displays the current image background color. Click it to select another color. If the image background style is transparent, the image background color is not used.
Image blink
For monochrome images, select this check box if the image is to blink at runtime. The image blinks twice per second.
Image back style
Click the down arrow and then click Solid or Transparent to specify the image’s background style. For color images that are not PNG with Alpha channel, if the Image back style is set to Transparent, any parts of the image that are black will be transparent.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal