Causes of runtime errors for the symbol indicator

At runtime these circumstances produce these error conditions:
Invalid values
If the Indicator tag value does not match any of the state values for the indicator, the indicator displays the error state.
Unassigned connections
If the Indicator connection is not assigned, the indicator displays the error state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal