Configure general properties of a momentary push button
After you set up the options in the
General
tab, click the States
tab to specify how the button looks in each state at runtime.To configure general properties of a momentary push button:
- In theMomentary Push Button Propertiesdialog box, in theGeneraltab, specify the following properties if needed:
- general appearance
- type of action the button initiates
- push button hold time
- touch margins
- audio (whether the button beeps at runtime)
Provide Feedback