Error state for the momentary push button
The error state is shown at runtime if one of the following is true:
- TheValueconnection is unassigned.
- The value of theValueconnection does not match one of the configured state values.
- The value of theIndicatorconnection does not match one of the configured state values.
Provide Feedback