Set up a connection for a gauge

Use the
Connections
tab to set up a connection for a gauge object.
To set up a connection for a gauge:
  1. In the
    Graphics
    editor, double-click the object to open the
    Gauge Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag or expression to the Value connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal